This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432: utility of erasing flash by command line

Part Number: IWRL6432
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Hi experts,

I need a function for erasing the whole flash, and I found "Format SFLASH" in settings & Utilities section in the UniFlash tool.

But in our production line, it can not use the GUI tool, it must be the command line used.

For burn-in images purpose, I can use 

{MMWAVE_L_SDK_xx_xx_xx_xx}\tools\boot\arprog_cmdline.py

which is the same as the Uniflash to satisfy our burn-in requirement in cmd line mode for our production line.

The path  {MMWAVE_L_SDK_xx_xx_xx_xx}\tools\ have no tool for erasing flash purpose, could you help to confirm?

If not, is there any way to satisfy the erasing flash in cmdline requirement?