Other Parts Discussed in Thread: AWR2243, AWR1843
Tool/software:
Hi,
I'm currently working on implementing the calibration process for the IWR6243 2-chip cascade device, as outlined in the following application note:
https://www.ti.com/lit/an/spracv2/spracv2.pdf?ts=1740429099901
This document includes detailed phase shifter accuracy plots for Gen 1 and Gen 2 devices (specifically, the AWR1843 and AWR2243). Is there a similar document from TI that provides such plots for the IWR6243?
Additionally, the application note provides TX phase shift calibration temperature correction LUTs for the AWR2243 (covering the 76–77 GHz and 78–81 GHz bands). Can TI share equivalent LUTs for the IWR6243 (60 GHz band)?
If not, could TI provide guidance on how to generate these phase shifter accuracy plots and temperature correction LUTs for our IWR6243 2-chip cascade setup.
Regards,
Attiya