Tool/software:
I use the EVM to realize an entry detection.
In order to create comparability with other sensors, I would like to use the log data from the mmWave Radar Visualizer.
However, these are only logged as raw data. What data format is used and how can I process this data?
Thank you very much and best regards
Tobias Hürtgen
<----------------[ VERSION INFO START ]---------------->
Platform : XWRL6432
RFS Firmware Version : 07.01.00.04
FECSS Lib Version : 03.01.08.01
mmWaveLink Version : 03.02.03.00
RFS Patch Version : 07.02.05.04
mmWave SDK Version : 05.05.03.00
<-----------------[ VERSION INFO END ]----------------->
<-------------[ CONFIGURATION INFO START ]------------->
sensorStop 0
channelCfg 7 3 0
chirpComnCfg 20 0 0 128 4 30 0
chirpTimingCfg 6 28 0 90 59.75
frameCfg 8 0 403 1 250 0
guiMonitor 2 2 0 0 0 1 1 0 0 0 0
sigProcChainCfg 64 8 2 0 4 4 0 .5
cfarCfg 2 4 3 2 0 12.0 0 0.5 0 1 1 1
aoaFovCfg -60 60 -40 40
rangeSelCfg 0.1 4.0
clutterRemoval 1
compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000
adcDataSource 0 adc_data_0001_CtestAdc6Ant.bin
adcLogging 0
lowPowerCfg 1
factoryCalibCfg 1 0 40 0 0x1ff000
mpdBoundaryBox 1 0 1.48 0 1.95 0 3
mpdBoundaryBox 2 0 1.48 1.95 3.9 0 3
mpdBoundaryBox 3 -1.48 0 0 1.95 0 3
mpdBoundaryBox 4 -1.48 0 1.95 3.9 0 3
sensorPosition 0 0 1.44 0 0
minorStateCfg 5 4 40 8 4 30 8 8
clusterCfg 1 0.5 2
baudRate 1250000
sensorStart 0 0 0 0
<--------------[ CONFIGURATION INFO END ]-------------->
<----------------[ DATA CAPTURE START ]---------------->
� 2d
����- P UU9s�; �>