Tool/software:
Hi,
According to AWR2944 EVM hardware design, we design our own board and AWR2944 EVM as belows:


and our PCB is as belows:
By road test, we compare our board and AWR2944 EVM board. We find a poblem for our board more noisy points are introduced. we think may be two factors, one is the manufacturing process of antenna,the other is the location of antenna.Though the hardware designs are identical, because of the different manufacture and different board material, that lead to different performances, is that right?What parameters or factors will affect antenna performance? By comparing the two boards we can see that:the antenna location of our own board is in the middle of the board, while in the AWR2944 EVM, the antenna loaction is in the left of the board. will more noisy points be introduced for different antenna location?If not, what other reasons will lead to more noisy points?
Thanks,
BR
Rata