This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AWRL1432BOOST-BSD: Sideband Data Capture with DCA1000 for BSD Demo

Part Number: AWRL1432BOOST-BSD


Tool/software:

Due to the BSD's demo large number of chirps and adc samples there have been issues with raw data capture with the DCA1000. To help alleviate this issue there are two steps to be taken

1) One cannot start the data collection before the sensorStart command has been sent

2) To help with BSD throughput there is a parameter for the DCA1000 that can be changed. Access the cf.json file present at this path.

    C:\ti\mmwave_studio_04_01_00_06\mmWaveStudio\PostProc\cf.json

    From there edit packetDelay_us to be 5us. This should help.

Note* Even with these changes the data still has a tendency to be corrupted about 10% of the time.