This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Two Lane Speed Detection Using AWR1843

Part Number: AWR1843


Tool/software:

Two Lane Speed Detection

Hello everyone, Im currently working on a system for detecting vehicle speed of maximum 40 km/h in two lanes only. From the out of box demo python file & the chirp config file, I've tried modifying the code & the parameters to get the desired results, but it only ends up me getting inconsistent speed detection only. Is there any way on how to solve this and if possible, any suggestions/feedback on this. If there is any sample code or even sample of the chirp config file that suits to my application, I would be more appreciate it. Any help/suggestion/feedback are welcomed & appreciated. Thank you very much.