This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: MMWave Studio 3.1.4.4

Part Number: DCA1000EVM

Tool/software:

I am having trouble connecting the mmWave studio software with the DCA1000EVM.  I have Matlab Runtime Engine v8.5.1 installed.  I have set the environment variables set to point to the runtime folder as well as the bin folder.  I can see all 6 COM ports are connected.  I have changed the ethernet port setting to 192.168.33.30 and 255.255.255.0 respectively.  When I open mmWave Studio I get and error that Runtime Engine is not installed.