Other Parts Discussed in Thread: IWR6843,
Tool/software:
Company is going to develop system for special vehicles for detection of small radars (30x30 cm) on a distance 100-150m. The questions are:1. Do the AWR1843 or IWR6843 are suitable for such usage? 2. Do those boards are able to detect targets by the following assumptions: - vehicle moving speed up to 60 km/h and drone flying speed directly towards vehicle -up to 30 m/sec? What specification we need to order to deploy the system? What conditions will be affect on radar performances' (rain, dust, fog????). How to order one radar with full installation manual to provide testing?