Other Parts Discussed in Thread: AWRL6432
Tool/software:
I am currently using the Life Presence Detection application included in the RADAR Toolbox 3.00.00.05, and I have encountered an issue.
When configuring antenna patterns other than EVM and AoP, the application does not provide accurate position estimation results.
Do you have any insights into the cause of this behavior?
I have confirmed that correct outputs are obtained when using Motion and Presence Detection OOB Demo provided by the MMWAVE_L_SDK5.x.
The antenna patterns for EVM and AoP are as follows. I would like to configure patterns other than these while ensuring proper operation.
The antenna pattern settings are being configured through antGeometryCfg.
- EVM: antGeometryCfg 0 0 1 1 0 2 0 1 1 2 0 3 2.418 2.418
- AoP: antGeometryCfg 1 1 1 0 0 1 1 3 1 2 0 3 2.5 2.5
Looking forward to your guidance.