Other Parts Discussed in Thread: MMWAVEICBOOST
Tool/software:
Hi all,
I am student currently working on a research project. Our project is building an FMCW mmWave radar system for vital sign detection (e.g., respiration and heartbeat monitoring).
Project Objective Summary: This project focuses on designing, simulating, and implementing a high-gain, high-isolation antenna system for 60 GHz FMCW radar, specifically targeting non-contact vital sign monitoring. The goal is to enhance TX/RX isolation to suppress self-interference and boost directional gain for improved sensitivity to chest motion within <1 meter. Signal validation will be performed using wavelet-based signal processing in MATLAB and Python.
We are intending to use the IWR6843ISK module and are designing a custom endfire antenna optimized for our specific sensing scenario. To integrate this custom antenna, we need to interface it with the radar sensor via an SMPM/SMA waveguide port.
We are reaching out to ask for support and guidance in the following areas:
1. Hardware Recommendation:
- Is the IWR6843ISK the most suitable module for our application, or would another radar EVM be more appropriate?
- Should we include the MMWAVEICBOOST board to help with interfacing, data acquisition, or firmware debugging?
2. External Antenna Integration:
- How can we properly modify the IWR6843ISK to disable or bypass the onboard antennas?
- Where on the board can we safely connect our SMPM/SMA port to the RF signal lines?
We greatly appreciate TI’s support and would love to collaborate to ensure the technical success of this academic project.
Best regards,
Van Phuoc Dang