Other Parts Discussed in Thread: IWR1843
Tool/software:
When I refer to TI's DEMO board to design the IWR1843 power supply, the 1.0V power supply track adopts the LC collocation in the figure below, and I found that IWR1843 frequent restarts in actual use, I think the voltage of 1.0v is too low, I increased the voltage output of the BUCK2 of the LP87524J to 1.2V, and still found that the IWR1843 restarts repeatedly, at this time, the voltage of the BGA pin near the IWR1843 is 970mv, which should not be restarted in theory. What causes the chip to reboot?
When I replace the 1.0uH inductor with a bead, the IWR1843 is working normally, and the voltage measured near the IWR1843 is 916mv, and the voltage is still lower but it doesn't restart, I don't know why this happens?