This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: Is there 100 ohm termination resistor for CSI integrated in AWR2944 SOC

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Tool/software:

Hi,

Does  100 ohm termination resistor  for CSI  integrated in the AWR2944 SOC , Is there any details available ?

  • Hi Kaviya, 

    when the awr2944 acts as a transmitter, 100ohm differential termination is expected externally or at the receiver's side. When 2944 is configured as CSI receiver, it does include internal 100ohm differential termination on the CSI input lanes this termination is integrated and can be enabled via software configuration.

    Regards,

    Aydin