Other Parts Discussed in Thread: IWR1642, IWRL6432AOP
Tool/software:
IWR1642: mmWave sensor radar based distance measure range about 5 meters
Can I achieve a resolution of 2 -5 mm?
I read that the resolution is about 21 mm which is not emough for my application.
Also, I saw something like "Platypus Passive Tags" that is able to do very accurate range calculations.
https://dl.acm.org/doi/10.1145/3583120.3586965
Can I achieve this with TI IWR1642: mmWave?
My purpose is to use mmWave to monitor a tunnel's width constantly over time using mmWave tech.
I have got the IWRL6432AOP EVAL module and hope to work with this.