This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: Bike Radar Demo

Part Number: IWRL6432BOOST
Other Parts Discussed in Thread: UNIFLASH,

Tool/software:

Hello,

I have a Question about the Bike Radar Demo.

I'm using UniFlash 9.1 and the radar_toolbox_3_00_00_05 with an IWRL6432BOOST.

I'm unable to flash the bike_radar_demo_6432.Release.appimage .

For example the mmwave_demo_xwrl6432.appimage works.

At both Flashes i have the following output errors.

[23.4.2025, 10:17:23] [ERROR] DEBUGSSM_0: Failed CPU Reset: Unsupported GTI Function.
[23.4.2025, 10:17:23] [ERROR] DEBUGSSM_0: GEL: Error while executing GEL_Reset(): Reset failed: retcode=-1 at GEL_Reset()
[23.4.2025, 10:17:23] [ERROR] CS_DAP_0: Failed CPU Reset: Unsupported GTI Function.
[23.4.2025, 10:17:23] [ERROR] CS_DAP_0: GEL: Error while executing GEL_Reset(): Reset failed: retcode=-1 at GEL_Reset()
[23.4.2025, 10:17:23] [ERROR] Cortex_M4_0: Failed CPU Reset: Unsupported GTI Function.
[23.4.2025, 10:17:23] [INFO] Cortex_M4_0: GEL Output: An error occurred while resetting. --1-n
[23.4.2025, 10:17:23] [ERROR] Cortex_M4_0: GEL: Error while executing GEL_Reset(): Reset failed: retcode=-1 at GEL_Reset()

However i can flash the mmwave_demo_xwrl6432.appimage with this output, so it maybe doesnt matter.

But I want to flash the bike appimage for fast velocity settings.

Can you help me?