This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460-Q1: PGA460-Q1

Part Number: PGA460-Q1
Other Parts Discussed in Thread: PGA460, ENERGIA, MSP-EXP430F5529LP

Tool/software:

the datasheet, I noticed it is possible to connect the PGA460 via various bus protocols, such as SPI, OWU, and USART. Would it also be possible to do this via UART?

Or do I need to connect them via SPI when the UART_ADDR is programmed in?

I am also curious if there is a C library for the PGA460 that can be easily used with other microcontrollers that may not be from TI.

Thanks in advance.