This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5013-Q1: DRV5013FA

Part Number: DRV5013-Q1

Tool/software:

We are going to select DRV5013FA, magnet ring generate alternating magnetic field,transistion angle.pptx

From -1.3mT to 1.3mT, the transition angle of magnet ring is 0.4deg? is this ok

  • Wei,

    Yes, this should work.  The small difference between switch points will result with a tighter tolerance from unit to unit where the output will toggle and a nearly ideal 50% duty cycle.  The potential down side is that if you manage to stop near the 0 crossing and have mechanical vibrations it is possible to have the output switch with very little motion.

    Thanks,

    Scott

  • what is max allowed transition angle  between switch points ?which one do you Suggest? thanks