Other Parts Discussed in Thread: LMP91002, ASH
Tool/software:
Dear team,
May I know how to configure the LMP91000 bias voltage for zero bias gas sensors.
I use LMP91002 with this sensor from Alphasense.
Regards
Hari
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear team,
May I know how to configure the LMP91000 bias voltage for zero bias gas sensors.
I use LMP91002 with this sensor from Alphasense.
Regards
Hari
Hari,
For non-biased gas sensors, you should use the LMP91002, it is specifically designed for non-biased sensors.
Regards
-Alex Thompson
Hari,
This is correct, the CE pin should be at 0V since it is a zero-bias sensor.

Thanks for sharing that app note, it's very helpful!
Thanks
-Alex Thompson
Hari,
You should not need to set any registers or activate the diagnostic functions to achieve zero bias. It should be as simple as connecting the CE pin of the sensor to the CE pin of the LMP91002. It may be a case where the CE pin isn't forced to 0V but just isn't forced to any voltage. Just direct connection with no additional settings should be sufficient for the CE pin.
Thanks
-Alex Thompson
Hi Alex,
Thanks for the confirmation.
""LMP91002 Configurable AFE for Low Power H2S and CO Sensing Applications"
I belive I can use it for other gases also.
I am working on a gas sensor node project which contains more than 16 gas sensors.
In this more than 8nos are electrochemical sensors with zero bias.
Below is the list of electrochemical gas sensors I am going to use.I believe this IC can be used for all not specific to H2S and CO
| Chlor (Chlorine, Cl₂) | Alphasense CL2-A1 | CL2-A1 |
| Ethylenoxid (Ethylene Oxide) | Alphasense ETO-A1 | ETO-A1 |
| Schwefelwasserstoff (Hydrogen Sulfide, H₂S) | Alphasense H2S-A1 | H2S-A1/H2S-D4 |
| Cyanwasserstoff (Hydrogen Cyanide, HCN) | Alphasense HCN-A1 | HCN-A1 |
| Phosphin (Phosphine, PH₃) | Alphasense PH3-A1 | PH3-A1 |
| Aceton (Acetone) | Alphasense PIDX-A-4000 | PIDX-A-4000 |
| Schwefeldioxid (Sulfur Dioxide, SO₂) | Alphasense SO2-A4 | SO2-A4 |
| Arsin (Arsine, AsH₃) | ES4-AsH3-1 | ES4-AsH3-1 |
| Methylmercaptan (Methanethiol, CH₃SH) | ES4-CH4S-100 | ES4-CH4S-100 |
| Formaldehyd (Formaldehyde, HCHO) | Gravity Formaldehyde Sensor | Gravity HCHO |
| Tetra-Chlor-Ethylen (Tetrachloroethylene) | Ion Science MiniPID 2 HS | MiniPID 2 HS |
| Tri-Chlor-Ethan, 1,1,1- (Trichloroethane) | Ion Science MiniPID 2 HS | MiniPID 2 HS |
| Tri-Chlor-Ethylen (Trichloroethylene) | Ion Science MiniPID 2 HS | MiniPID 2 HS |
| Phosgen (Phosgene, COCl₂) | Sensorix COCl2 | Sensorix COCl2 |
| Hydrazin (Hydrazine, N₂H₄) | Sensorix N2H4 1 | AN181400 |
| Ammonia (NH₃) | SGX-4NH3-1000 | SGX-4NH3-1000 |
| Fluorwasserstoffsäure (Hydrogen Fluoride, HF) | SGX-HF-10 | SGX-HF-10 |
Hari,
This IC can be used with other zero bias electrochemical sensors, not just H2S and CO.
Thanks
-Alex Thompson