Tool/software:
Hi Team, seeking for some insights.
I would like to sincerely explain my situation and kindly ask for further assistance.
This XDS110 issue is part of a university research project involving the IWRL6432 LaunchPad. I’m a student working on a mmWave sensing system, and I accidentally executed a firmware update command while the board was not properly connected. Since then, I’ve spent weeks attempting to recover the board using all available troubleshooting methods, including:
- Multiple USB cable and port swaps (direct to motherboard USB 2.0)
- System cold shutdown and USB power resets
- Holding the reset button while inserting USB
- Driver cleanup and reinstallation (including Stellaris DFU)
- Trying on multiple PCs
- Following both the XDS110 recovery guide and JTAG troubleshooting checklist
Currently, the board only appears in Device Manager as:
Stellaris Device Firmware Upgrade (Code 45)
There is no USB response or sound, and the xdsdfu tool still returns "Found 0 devices". This clearly indicates that the onboard XDS110 is stuck in DFU mode but unable to communicate. I believe the bootloader or firmware is corrupted in a way that cannot be recovered without a second debugger, which I do not have access to.
This board is used in my coursework and I do not have the resources to reflash the XDS110 via JTAG or purchase a new LaunchPad at the moment.
Thank you.
-Mark