Other Parts Discussed in Thread: DCA1000EVM, UNIFLASH
Tool/software:
Hi TI team,
I'm working with the AWR2944EVM and DCA1000EVM and using the open-source ROS package xwr_raw_ros, which appears to require SDK version 4.2.0, based on the .cfg files provided (e.g., % Created for SDK ver:04.02).
Currently, my radar is running firmware from SDK 4.7, and when I run the config through the ROS interface, the device responds only with repeated CCCCCCCCCCC and never sends Done. I suspect this is due to SDK incompatibility.
My questions are:
1. Is it safe to flash the AWR2944EVM from SDK 4.7 to SDK 4.2 using UniFlash?
2. Can I later re-flash it back to SDK 4.7 without any issues or side effects?
3. Are there any conditions, or limitations. I should be aware of when switching SDK versions on this platform?
Thanks in advance for your help!