This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: Exporting Post-Processing Data from mmWave Studio in Custom Formats

Part Number: AWR2944EVM
Other Parts Discussed in Thread: DCA1000EVM

Tool/software:

We are currently developing with the AWR2944EVM and have successfully interfaced it with the DCA1000EVM to capture raw ADC data. Using mmWave Studio, we are able to extract and visualize this raw data without issues. However, we are encountering difficulties when attempting to export the data into a custom format—for example, saving range-Doppler and angle-range heatmaps as JPEG or PNG images for further post-processing.

Additionally, we have not been able to locate any reference source code or documentation detailing the processing pipeline used to generate key visual outputs such as range profiles, Doppler maps, and angle-of-arrival (AoA) plots, as produced by the mmWave Studio post-processing tools.

Our goal is to replicate and extend these processing steps independently, outside of mmWave Studio. To facilitate this, we would greatly appreciate access to any relevant source code, example scripts, or SDK documentation that outlines the complete signal processing chain from raw ADC data to the final plots.

kindly request your assistance in guiding us to the appropriate tools, libraries, or repositories that support this advanced level of data processing, particularly for AWR2944EVM.

  • Hi,

    Once you have the plots you can select File>Save As> Select desired format from "Save as type" menu.

    Unfortunately, the source code for post-processing is not available. However, the steps involved are quite standard for Radar Signal Processing and no advanced processing is performed.

    Regards,

    Shailesh