Other Parts Discussed in Thread: TMP118, , , TMP117, ISOTMP35
Tool/software:
I am using a competeitor's device to measure the temperature of a (largely) metallic block. It's a WSON type pacakage and the board is mounted upside down so that when secured with a blob of thermal epoxy, the top of the IC is in contact with the block. We have had issues with this design (for different reasons other than the mounting method) which has led me to experiment with the TMP118/9EVM boards and they do not show the same issue which is great, but I am not sure if we can use the same technique for mounting as we currently do.
I have read SNOA986A and that is based upon the mounting of the PCB the right way up, so that the PCB layer is between the IC and the sensed object which seems as if you're building in errors from the start which need to be overcome.
I would like to mount it in the following way - is there a reason why this would not be considered appropriate?
We have been using this technique without issue to date with our existing IC.

It'd be great to discuss this with an FAE if that were possible?
Thanks