This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP63-Q1: Thermistor - terminal connection

Part Number: TMP63-Q1


Tool/software:

Hello,

For TMP63-Q1 can I connect the sensor like this?

Instead of the typical application which Thermistor's - terminal connected to the GND?

Best regards,

Egemen

  • Hi Egemen,

    I would be careful with your chosen configuration, it should be tested first to make sure the results are in datasheet spec. We do recommend swapping the positions of the bias resistor and the PTC, like in the 2nd diagram. You can place the capacitor in parallel with the PTC though. At DC the capacitor will act as an open circuit, so it wouldn't siphon off current from the PTC.

    Regards

    -Alex Thompson