Other Parts Discussed in Thread: , UNIFLASH
Tool/software:
We are planning to develop a people presence and distance detection system within a defined zone of approximately 2 x 2 meters, using the IWR6843AOP mmWave Radar (MPN: IWR6843ARQGALPR). The radar will operate in standalone mode and communicate with a Raspberry Pi Compute Module 5 via UART.
For power management, I plan to use the LP87524JRNFRQ1 PMIC as per the reference design.
I have several questions regarding the hardware integration and firmware development:
1. Use of Mission AOP Board Without Breakaway Board
I noticed that the IWR6843AOPEVM consists of two sections: the Mission AOP Board and a Breakaway Board. Based on my understanding, the Mission AOP Board can function independently without the Breakaway Board.
Could you please confirm this?
2. Firmware Upload in Custom Board Design
We are designing our own board similar to the Mission AOP Board, which includes the mmWave sensor, PMIC, QSPI Flash, USB-to-UART, and crystals.
-
How can we upload the firmware in this custom design?
-
Since the PMIC requires control via I2C by the IWR6843AOP, how can the sensor initiate this sequence without having firmware preloaded?
3. Flashing the QSPI NOR Memory
Is it necessary to pre-flash the QSPI NOR memory before soldering it onto the PCB, so that the IWR6843AOP can boot from it successfully?
4. PMIC and Bootloader Support
Alternatively, does the IWR6843AOP have any pre-programmed bootloader or firmware to configure the PMIC for initial boot and enable UART functionality for firmware upload using tools like UniFlash?
5. Communication Interface Recommendation (UART vs SPI)
Which interface is recommended between UART and SPI for data communication between the IWR6843AOP and Raspberry Pi CM5, considering performance and stability?
6. Deployment in Metal-Rich Environment (Clean Room)
The sensor will be deployed in an OHT clean room environment, where metallic structures are likely to surround the sensor within 1 meter.
-
Will the sensor be able to accurately detect people presence and distance in such an environment?
-
Are there any configuration or shielding recommendations to improve performance in metal-heavy surroundings?
7. Sensor Protection Design
We plan to enclose the sensor in a plastic box and are considering placing a glass panel with a 2–3 mm air gap directly above the radar module (Above AOP Antenna).
-
Would this affect the radar performance?
-
Are there recommended materials or design guidelines for covering and protecting the sensor without interfering with its detection capabilities?
I would appreciate your expert guidance on the above points to ensure a successful integration and deployment of the IWR6843AOP radar module.
Thank you for your support.