Other Parts Discussed in Thread: TMP112-Q1, TMP102
Tool/software:
Hello:
The specification sheet of TMP102-Q1 shows the accuracy without calibration. May I ask how much accuracy can be achieved after calibration? Additionally, what is the operational mechanism of calibration? thank you!!!
Accuracy Without Calibration:
– 2°C (Maximum) From –25°C to 85°C
– 3°C (Maximum) From –40°C to 125°C