This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: OPT3001

Part Number: OPT3001


Tool/software:

I am using the OPT3001 component and am very satisfied
A customer of mine asked for the component's output to be SPI instead of I2c

1. Do you have a component with an SPI output?
2. Can the OPT3001 can be converted to SPI?
3. If so, which component can be used.


Thank you very much
Yehonatn.
 
  • Hi Yehonatan,

    Unfortunately, we do not have any devices that support communication for SPI. All of our devices use I2C only and will continue to be for the foreseeable future. Is there a reason why you are using specifically SPI? Could I2C work for your use case?

    Thanks,
    Daniel