Tool/software:
I want to run area_scanner or something similar on my IWR6843ISK device. I have loaded the binary on my device. Then I load the area_scanner config file, which has some very specialized commands.
Specifically: heatmapGenCfg and staticDetectionCfg. These I need to be able to identify static humans walking into a scene. I want to be able to run a visualizer in python (not in Matlab). It seems the
visualizer for area_scanner is a matlab program, not a python program. If I try to use the area_scanner config with Out_of_the_box binary, it does not recognize those specific config files for static detection. Is there a binary
that will run on Industrial_visualizer or something similar that is in python, and also recognize those config commands.. Industrial_visualizer cannot parse area_scanner binary output because the format out is different.
My project runs on a computer that is very specialized using linux and only runs python.
Please help!
Thanks,
larry