Tool/software:
Hello,
I am trying to make a function which will set the Configurations, other than the already available CLI_Task(), which monitors the UART port for configurations. I am using the long_range_people detection demo for the same. The issue I am facing is that when I call the extended function for "flushCfg", it calls the SDK internal function MMWave_flushCfg(). My Code is crashing after that point. I am stuck as to why that could be the case as MMWave_flushCfg() is defined in the SDK only.
If anyone can provide any insights that will be very helpful. Also, please mention anything that I need to clarify more.
Thanks & Regards,
Prishat