This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: Query for ChirpTxMimoPatSel cfg: sd5.2.0 against 5.5.3

Part Number: IWRL6432BOOST

Tool/software:

Hi,
For sdk  xWRL6432 MMWAVE-L-SDK 05.02.00, for IWRL6432BOOST ES1.0, for below cfg: it says only 1 and 4 are supported?

ChirpTxMimoPatSel

Only BPM is supported in current OOB Demo.
0 - TX BPM MIMO pattern disabled
1 - TDMA_2TX pattern
4 - BPM_2TX pattern

Since in 5.5.3 SDK, I see 0 is not supported.

Can you confirm if it's correct for 5.2.0 SDK or not?

  • Hello, 

    Which out of box demo version are you using (mmwave demo or motion and presence detection)? For mmWave demo, only BPM is supported (4) for motion and presence detectiono demo both options are supported (1 or 4).

    Best regards,

    Josh