Tool/software:
Hello
I am making a product using TMAG3001 by referring to TMAG3001_Exmaple_Code provided in this link. :www.ti.com/.../TMAG3001
I am interested in recognizing the angle change of the magnet,
So I referred to the WOC_ANGLE_EXAMPLE area.
However, my product is battery-based, so I have to wait in low power when the magnet is not rotating.
So I tried changing this part to enter the WakeAndSleep Mode.
But when I do this, I get endless interrupts with a cycle of about 2~5ms.
This is the exact opposite of what I intuitively think.
Is there some additional setup that I'm missing? or Can't I use low power performance and WOC_ANGLE feature at the same time?
Please advice.
Regards.