This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: Query with range-azimuth (heatmap) TLV for LSDK 5.5.3

Part Number: IWRL6432BOOST


Tool/software:

Hi,
For MMWave_SDK , we have the heatmap tlv for range-azimuth like this

Type Identifier

Type Value Length Value
4 MMWDEMO_OUTPUT_MSG_AZIMUT_STATIC_HEAT_MAP (Range FFT size) x (Number of “azimuth” virtual antennas) x (4 Bytes) Samples to calculate static azimuth heatmap (no moving object signal). This is a 2D FFT array in range direction (x[numRangeBins][numVirtualAntAzim]), at doppler index 0.

The antenna data are complex symbols, with imaginary first and real second in the following order:

Imag(ant 0, range 0), Real(ant 0, range 0),…,Imag(ant N-1, range 0),Real(ant N-1, range 0)

Imag(ant 0, range R-1), Real(ant 0, range R-1),…,Imag(ant N-1, range R-1),Real(ant N-1, range R-1)



But for LSDK , we have 
"The matrix is arranged as X[rangeInd*azimuthFftSize + azimuthInd], rangeInd = 0, numRangeBins - 1, azimuthInd = 0, azimuthFftSize – 1"

So we directly get the magnitude for each bin(per range/ per angle), and we don't need to do any post processing
If I need to plot, I can directly do this(Psedo code below)

% Suppose you read `data` from TLV binary
heatmap = reshape(data, [numAzimuthBins, numRangeBins])';
heatmap = fliplr(heatmap); % Optional: flip angle direction
plot(heatmap);

- Is my understanding correct?