This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Need Help for Custom PCB Design

Part Number: AWR1843
Other Parts Discussed in Thread: TM4C1294NCPDT,

Tool/software:

Hello Everyone

Hope everyone is doing well.

So I am working on a radar PCB Design taking reference from AWR1843BOOST Evaluation board. So in my deign I have made some changes such that it makes the PCB becomes cost effective.

First, I have to ask about the TM4C1294NCPDT IC which is used as a debugging interface similar to the XDS110 family now in my design I have removed the TM4C1294NCPDT IC now can I still debug the PCB using JTAG??

Second, So for debug and flash mode changing we need to change the SOP states using a switch as in the AwR1843BOSST EVKT now for my design I have taken the SOP inputs from a connector externally so will it be okay to take this input externally??

Third, For the debug interface I have used a separate 6 pin connector as well as for the RS232 as a 4 pin connector and one more 18 connector in which I have taken the main VIN supply of 12V for the PCB, the SOP inputs that I have talked about earlier in the above question, UART TX RX lies and the MSS_LOG DSS_LOG connection as well as few Ground pins. Now is it okay to take all these data lines into a single connector???

Fourth, In this design on the AWR1843 Chip their is one pin, numbered as P4 and named as SYNC IN so do I need to connect it while performing the debug operation??

Lastly I am attaching my Schematic design below as a PDF format, I would love to get a review from your side and what are changes will be needed please let me know such that all the points would be covered and my design would be error free. I have tried to write some of the key question above. So I want get review before I send my design for Fabrication and assembly I want to make sure the board works fine after the manufacturing.

Regards

Ratul