This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC3022: HDC3022: Application question regarding HDC3022

Part Number: HDC3022
Other Parts Discussed in Thread: HDC3021

Tool/software:

Hi Team,

I want to double check with you whether HDC3021/3022 can measure the ambient temperature on TWS or smartwatch application? If so, does the measured temperature will be affected by the body temperature? Thanks.

BRs.

Frank 

  • Hello Frank,

    It is highly likely the HDC3021/3022 will be affected by body temperature due to the device being in direct contact with a user's skin. This can be mitigated by adding a cutout around the sensor as well as keeping it away from copper planes, however this may be difficult in a space-contricted design such as a smartwatch or TWS.

    I also see you posted the same question the day before and will close that thread.

    Regards,

    Harry