Other Parts Discussed in Thread: IWRL6432
Tool/software:
Hello TI Team,
I have another question about the IWRL6432 SPI RAW DATA.

So did I understand right, that the ADC Data, which I get over SPI ist captured directly after the IF? So there is no calculation done for example RangeBias und RX Channel Phase Correction?
I'm just wondering because the configuration file seems to define a complete signal processing chain.
sensorStop 0
channelCfg 7 3 0
chirpComnCfg 8 0 0 128 1 15 1
chirpTimingCfg 6 40 2 240 57
frameCfg 600 0 19860 1 40 800
guiMonitor 2 1 0 0 0 1 0 0 0 0 0
sigProcChainCfg 32 2 1 0 4 4 0 15
cfarCfg 2 8 4 3 0 12.0 0 0.5 0 1 1 1
aoaFovCfg -60 60 -40 40
rangeSelCfg 0.1 12.0
clutterRemoval 1
compRangeBiasAndRxChanPhase 0.06559 -0.12472 -0.67939 0.51038 0.58357 -0.53357 -0.62848 0.06786 0.94560 -0.60156 -0.79883 0.57553 0.77879
adcLogging 2
lowPowerCfg 0
factoryCalibCfg 0 1 40 0 0x1ff000
mpdBoundaryBox 1 0 1.48 0 1.95 0 3
mpdBoundaryBox 2 0 1.48 1.95 3.9 0 3
mpdBoundaryBox 3 -1.48 0 0 1.95 0 3
mpdBoundaryBox 4 -1.48 0 1.95 3.9 0 3
sensorPosition 0 0 1.44 0 0
minorStateCfg 5 4 40 8 4 30 8 8
majorStateCfg 4 2 30 10 8 80 4 4
clusterCfg 1 0.5 2
profileSwitchCfg 0 25 25
sensorStart 0 0 0 0
Furthermore I want to get the ADC Smaples not in Burst Mode, so I can measure high velocitys. But it seams that when I turn NumberofBursts in Frame to 1, it doesn't work anymore?
***WARNING*** Sensor did not respond with done
Response: b'DOA DPU config return error:-2801 \n'