Other Parts Discussed in Thread: IWR1843, DCA1000EVM
Tool/software:
Currently Iam using IWR1843 (without DCA1000EVM), and configuring the output in mmWave Demo visualizer,
1. I want to Configure the sensor to detect stationary and moving (objects, humans, bikes, cars, trucks) up to 75 meters, with maximum Field of View (FoV), and export processed detection data using (no DCA1000EVM).
2. What parameters in the configuration (e.g., chirp design, profileCfg) need to be adjusted?
3. How can I save the processed output data (i.e., detection points with range, velocity, etc.) into a CSV or Excel-compatible format using the mmWave Demo Visualizer?
4. What is the maximum range and maxiimum fov (Horizontal field of view and vertical field of view) that i can configure using IWR1843 boost?
5. Anyother tools to visualize the output apart from point clouds? what other ouputs can be visualized apart from point cloud without DCA1000EVM
6. Can i live stream the output to save or process further, if yes please suggest any micro controllers which help or compaitable?