This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: Timmer IC Choice with 2-output frequencies

Part Number: TDC7200


Tool/software:

Timmer Choice for TDC 7200: I am looking for the right timer IC to use with the TDC 7200 for the 8MHz timer input.

I would like to have 2-different outputs so I can use the 2nd output at a different frequencies for a different IC.