Tool/software:
Hello,
I have been using the Industrial_Visulaizer.exe of the radar toolbox with the out-of-the-box demo of an x432 radar. Everything works great. I see the point cloud and the bounding box as we move around.
Then I tried the Python source code version instead of the .exe file. The visualizer starts and with the same config file as before I can display the bounding box moving around but the point cloud are not showing up.
I looked into gui_threads.py and I can see what appear to be a correct point cloud data being passed to self.scatter.setData around line 199 but I do not see anything in the display.
Where should I look next?
Thanks
Pascal