Tool/software:
Hello,
I would like to inquire about the distance between the de-cap and the AOP pins
During the PCB layout process using the AWR1843AOP chip, due to space constraints, the decoupling capacitors (DECAPs) for pins E1 and J1 were placed at distances of 5.6mm and 9mm, respectively (please refer to the attached photo).
We are aware that it is recommended to place decoupling capacitors as close to the pins as possible; however, due to physical limitations, we were unable to do so.
I would like to request your review on the following points:
1.Please confirm whether the current distances between the DECAPs and the pins (5.6mm and 9mm) could cause any issues with electrical stability.
2.If there is a recommended maximum allowable distance between the DECAP and the pin according to TI (Texas Instruments) guidelines, I would appreciate it if you could share this information.
I look forward to your response.
Thank you