This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3004: Need Details on Optomechanical Design Aspect

Part Number: OPT3004

Tool/software:

Hii Team,

Is optomechanical Design Mandatory for OPT 3004 Sensor to use?

Regards,

Karthik

  • Hello Karthik, 

    If unit is uncovered or there is no opaque backing to cover glass then there is no need to design the window dimensions as then there is no need for a window.  However when there are object that obscure the light to be sampled from the sensor than these need to be considered to understand the limitations of the system.  

    In short: TI encourages customers to carefully consider optomechanical design for best results. 

    Thank you, 

    Joseph