This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOPEVM: IWRL6432 Sensor

Part Number: IWRL6432AOPEVM
Other Parts Discussed in Thread: IWRL6432

Tool/software:

What is the field of view for the IWRL6432 radar senor both vertically and horizontally? Also, can I scale it down to 5 degrees or less for one of the fields? I am needing to create a very thin field that spans 60-90 degrees, like a curtain.

If there is a better sensor for this I am open to suggestions. I do need mm accuracy and at least 100 readings per second and at least 5 m detection length in a 2D plane.