This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: AWR1243BOOST

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR1243

Tool/software:

Hello,

I am setting up AWR1243 and DCA1000. All the connections have been successfully done as pointed out in the guide. 5V power supplies with >2.5A current, micro USB connections, and ethernet connection. After setting them up and verify that SPO0 and SOP1 are connected, I changed the IPV4 address. Screenshot attached for reference.:


After doing all this process, I started the mmwave studio, and successfully set up all the parameters in 'Connection', 'StaticConfig', 'DataConfig' and 'SensorConfig' tabs. In the output tab, I all the configuration was successfully done. However, when I clicked the 'Setup DCA1000' button and clicked in Connect, Reset and Configure button, I get an error in the output tab that 'Unable to read FPGA Version'. I repeated this process multiple times, but am getting the same error.

The output commands are:

[21:37:01] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 30)
[21:37:01] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[21:37:01] [RadarAPI]: Sending fpga command to DCA1000
[21:37:11] [RadarAPI]:
[21:37:11] FPGA Configuration :
[21:37:11] Timeout Error! System disconnected
[21:37:11] [RadarAPI]: Sending record command to DCA1000
[21:37:21] [RadarAPI]:
[21:37:21] Configure Record :
[21:37:21] Timeout Error! System disconnected
[21:37:21] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
[21:37:21] [RadarAPI]: Sending fpga_version command to DCA1000
[21:37:31] [RadarAPI]:
[21:37:31]
[21:37:31] Unable to read FPGA Version. [error -5]

Please How can i desactivate Firewall ? and also reflashing my fpga without using diamond because it's not free ?

Thanking you in anticipation

Regards

Fatima-ezzahraa