This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Maximum frame rate for IWR6843ISK

Part Number: IWR6843ISK


Tool/software:

Hi,

I have a IWR6843ISK. Currently I am running radar module at 5Hz(200ms) frame periodicity. What is the maximum frame rate that I can be achieved?

I am trying to run radar at 20Hz frame rate/50ms frame periodicity. Is it possible to run 4 radars as a node at 20Hz frame rate on a CAN bus? I have a CAN bus where I have connected 4 radars as a node. 

Thanks,
Manoj