Part Number: OPT4060
Tool/software:
Hello,
I am using the OTP4060 to measure the light in a display and I've noticed that when I set the display to the dimmest setting I can read very low counts (EXP = 0, MANTISSA ~28-48) when I set the conversion time to 200ms or faster. Unfortunately the 400ms and 800ms conversion times are continuously reporting 0 (which surprises me, as these are supposed to be used in low light settings).
This light source is PWMING at 0.19% (5/2667) duty cycle. I have the range set to auto-range. I have noticed that although the interrupt signal is going low when expected (after 4 full conversion times), the counter for each color is not incrementing.
Can you please explain why the slowest conversion times are reporting all 0s?