This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Heat sink imaged

Part Number: AWR2243

Tool/software:

I put a small 0.25inch tall aluminum heatsink on my MMWAVCAS-RF-EVM, and it appears to be producing a large peak in the data, how can this be avoided? Do I have to mask out the close range bins?

  • Hi,

    If possible, could you use a non-metallic heatsink or thermal pad instead? If a metal is required, relocate or shield it with absorber so it's out of the direct line of sight of the antenna. You could also mask the close-range bins during signal processing but that's more of a workaround than a true fix.

    Regards,

    Aydin