This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: Converting mmWave studio configuration into a configuration file

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Tool/software:

Hi,

I defined the following configuration in the mmWave studio and I see the configuration works. I see that because the studio is able to generate and show me a dump using PostProc:

In the configuration that I built I tried to get maximum possible SNR for a single Tx operating

Now I converted the configuration into the following configuration file:

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 15 0
adcCfg 2 0
adcbufCfg -1 1 1 0 1
lowPower 0 0
profileCfg 0 77 10 10 140 0 0 2.8 1 511 4200 0 0 30
chirpCfg 0 0 0 0 0 0 0 15
frameCfg 0 0 255 0 511 40 1 0
lowPower 0 0
guiMonitor -1 2 0 0 0 0 0
antGeometryCfg 1 0 1 1 1 2 1 3 0 2 0 3 0 4 0 5 1 4 1 5 1 6 1 7 1 8 1 9 1 10 1 11 0.5 0.8
cfarCfg -1 0 3 16 0 0 1 15 0 7 0 1
cfarCfg -1 1 3 16 0 0 1 15 0 7 0 1
compressionCfg -1 1 0 0.5 8
intfMitigCfg -1 15 18
localMaxCfg -1 6 40
ddmPhaseShiftAntOrder 0 2 3 1
antennaCalibParams 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1
measureRangeBiasAndRxChanPhase 0 1.5 0.2
aoaFovCfg -1 -90 90 -90 90
calibData 0 0 0
sensorStart

However, when I use the online visualizer, trying to run this configuration file, seams that the visualizer "doesn't like" the configuration and don't want to run it.

What is wrong in the config file that I built?

Thank you for help,

Arie