Part Number: TMAG5170
Tool/software:
I have a design that needs to track the proximity of a magnet in close proximity of this sensor. The maximum range of motions is around 4mm and the maximum distance away from the sensor will be 15mm.
The event can be as fast as 0.6ms, and I need to detect this event with reasonable resolution. The TMAG running over SPI shows a 10mhz bandwidth and 20ksps sampling. is it reasonable to expect this device to provide an adequate resolution of the event ? Would ideally be tracked in 2 axis but 1 axis will do and if this can provide the resolution, can the Alert be setup to trigger based on this event being detected