This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: I Changed the config file using ROS2 and i cant get the pointcloud data anymore.

Part Number: IWR6843AOP


Tool/software:

Hello, i'm using a IWR6843AOP radar with ROS2 on an ubuntu 22.04 system. Since today i was using the cfg file named as "6843AOP_Standard.cfg" but i changed so i can have more range.Since then i get this log when i'm running the "ros2 launch ti_mmwave_rospkg 6843AOP_Standard.py" 

[INFO] [launch]: All log files can be found below /home/nefeli/.ros/log/2025-06-27-14-42-26-930812-nefeli-desktop-20009
[INFO] [launch]: Default logging verbosity is set to INFO
[INFO] [mmWaveCommSrv-2]: process started with pid [20012]
[INFO] [mmWaveQuickConfig-3]: process started with pid [20014]
[INFO] [ParameterParser-4]: process started with pid [20016]
[INFO] [DataHandlerClass-5]: process started with pid [20018]
[INFO] [ConfigParameterServer-1]: process started with pid [20010]
[INFO] [rviz2-6]: process started with pid [20020]
[mmWaveQuickConfig-3] [INFO] [1751024547.121866120] [rclcpp]:
[mmWaveQuickConfig-3]
[mmWaveQuickConfig-3] ==============================
[mmWaveQuickConfig-3] mmWave ROS Driver is starting
[mmWaveQuickConfig-3] ==============================
[mmWaveQuickConfig-3]
[mmWaveQuickConfig-3] [INFO] [1751024547.128011275] [rclcpp]: mmWaveQuickConfig: Configuring mmWave device using config file: /home/nefeli/Desktop/mmwave_ti_ros/ros2_driver/install/ti_mmwave_rospkg/share/ti_mmwave_rospkg/cfg/6843AOP_Standard.cfg
[mmWaveQuickConfig-3] [INFO] [1751024547.159097892] [rclcpp]: File was opened
[DataHandlerClass-5] [INFO] [1751024547.172289866] [rclcpp]: DataUARTHandler Read Thread: Port is open
[mmWaveCommSrv-2] [INFO] [1751024547.183460902] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'sensorStop'
[mmWaveCommSrv-2] [INFO] [1751024548.184982542] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[rviz2-6] [INFO] [1751024548.191002060] [rviz2]: Stereo is NOT SUPPORTED
[rviz2-6] [INFO] [1751024548.191215059] [rviz2]: OpenGl version: 4.6 (GLSL 4.6)
[mmWaveCommSrv-2] [INFO] [1751024548.200990620] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'flushCfg'
[rviz2-6] [INFO] [1751024548.236241966] [rviz2]: Stereo is NOT SUPPORTED
[ParameterParser-4] [INFO] [1751024549.190089459] [rclcpp]:
[ParameterParser-4]
[ParameterParser-4] ==============================
[ParameterParser-4] List of parameters
[ParameterParser-4] ==============================
[ParameterParser-4] Number of range samples: 224
[ParameterParser-4] Number of chirps: 16
[ParameterParser-4] f_s: 7.000 MHz
[ParameterParser-4] f_c: 62.300 GHz
[ParameterParser-4] Bandwidth: 3200.000 MHz
[ParameterParser-4] PRI: 83.000 us
[ParameterParser-4] Frame time: 33.333 ms
[ParameterParser-4] Max range: 10.493 m
[ParameterParser-4] Range resolution: 0.047 m
[ParameterParser-4] Max Doppler: +-4.831 m/s
[ParameterParser-4] Doppler resolution: 0.604 m/s
[ParameterParser-4] ==============================
[ParameterParser-4]
[mmWaveCommSrv-2] [INFO] [1751024549.201190700] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024549.217685740] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'dfeDataOutputMode 1'
[ParameterParser-4] cannot publish data, at ./src/rmw_publish.cpp:62 during '__function__'
[ParameterParser-4] destroy_client() failed to delete datareader, at ./src/rmw_client.cpp:92 during '__function__'
[ERROR] [ParameterParser-4]: process has died [pid 20016, exit code -11, cmd '/home/nefeli/Desktop/mmwave_ti_ros/ros2_driver/install/ti_mmwave_rospkg/lib/ti_mmwave_rospkg/ParameterParser --ros-args -r __node:=ParameterParser --params-file /tmp/launch_params_6331k2wj --params-file /tmp/launch_params_n9249jco'].
[mmWaveCommSrv-2] [INFO] [1751024550.217944183] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024550.234828517] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'channelCfg 15 7 0'
[mmWaveCommSrv-2] [INFO] [1751024551.234667739] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024551.252386023] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'adcCfg 2 1'
[mmWaveCommSrv-2] [INFO] [1751024552.252648006] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024552.269612279] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'adcbufCfg -1 0 1 1 1'
[mmWaveCommSrv-2] [INFO] [1751024553.269977234] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024553.286696730] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'profileCfg 0 60 43 7 40 0 0 100 1 224 7000 0 0 30'
[mmWaveCommSrv-2] [INFO] [1751024554.286953355] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024554.303787158] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 0 0 0 0 0 0 0 1'
[mmWaveCommSrv-2] [INFO] [1751024555.304259369] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024555.321379935] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 1 1 0 0 0 0 0 2'
[mmWaveCommSrv-2] [INFO] [1751024556.321584801] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024556.337572461] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 2 2 0 0 0 0 0 4'
[mmWaveCommSrv-2] [INFO] [1751024557.337834474] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024557.354684822] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'frameCfg 0 2 16 0 33.333 1 0'
[mmWaveCommSrv-2] [INFO] [1751024558.354601984] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024558.371106047] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'lowPower 0 0'
[mmWaveCommSrv-2] [INFO] [1751024559.371291949] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024559.387652102] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'guiMonitor -1 1 0 0 0 0 0'
[mmWaveCommSrv-2] [INFO] [1751024560.387637286] [rclcpp]: mmWaveCommSrv: Received response from sensor: ''
[mmWaveCommSrv-2] [INFO] [1751024560.404627670] [rclcpp]: mmWaveCommSrv: Sending command to sensor: 'cfarCfg -1 0 2 8 4 3 0 15 1'
^C[WARNING] [launch]: user interrupted with ctrl-c (SIGINT)
[DataHandlerClass-5] [WARN] [1751024560.623420994] [rclcpp]: Stopping Threads
[mmWaveCommSrv-2] [INFO] [1751024560.623493317] [rclcpp]: signal_handler(signum=2)
[rviz2-6] [INFO] [1751024560.623414914] [rclcpp]: signal_handler(signum=2)
[ConfigParameterServer-1] [INFO] [1751024560.623441187] [rclcpp]: signal_handler(signum=2)
[mmWaveQuickConfig-3] [INFO] [1751024560.623942997] [rclcpp]: signal_handler(signum=2)
[mmWaveQuickConfig-3] [WARN] [1751024560.625383178] [rclcpp]:
[mmWaveQuickConfig-3]
[mmWaveQuickConfig-3] ==================================
[mmWaveQuickConfig-3] mmWave ROS Driver is shutting down
[mmWaveQuickConfig-3] ==================================
[mmWaveQuickConfig-3]
[mmWaveQuickConfig-3] terminate called after throwing an instance of 'rclcpp::exceptions::RCLError'
[mmWaveQuickConfig-3] what(): failed to create guard condition: the given context is not valid, either rcl_init() was not called or rcl_shutdown() was called., at ./src/rcl/guard_condition.c:67
[INFO] [ConfigParameterServer-1]: process has finished cleanly [pid 20010]
[INFO] [DataHandlerClass-5]: process has finished cleanly [pid 20018]
[INFO] [rviz2-6]: process has finished cleanly [pid 20020]


I changed back to the original cfg but i was still getting this error and no Pointcloud.

I rebuild the workspace but again nothing happens. Should i've do something else? Should i reflash the binary to the radar?

Thank you.

  • Hello,

    The response should be something like: mmWaveCommSrv: Received response from sensor: ''Done".

    What this means is that the issue is exclusively between communication of the mmWaveSensor and computer. After flashing your EVM in flashing mode, did you set it to functional mode? You can also confirm mmWaveSensor and computer communication via a terminal emulator like PuTTY or TeraTerm, where you can connect to the device and send those same configuration lines like "channelCfg 15 7 0" You should see a "Done" afterwards.

    EVM Setup Operational Modes User Guide

    Best Regards,

    Pedrhom