Tool/software:
Hello TI Team,
I am working with the AWR1843AOPEVM and have flashed the Medium Range Radar (MRR) demo binary, enabling only MRR mode.
-
I tested the radar in open space up to 80 meters.
-
The detection results are accurate and reliable within the default configuration.
-
However, the Field of View (FOV) is very limited for my application.
Application Requirement:
For my use case, I need the radar application that:
-
Detect any object within 50 meters
-
With lateral FOV of ±1.7 meters from the radar’s centerline (i.e., total 3.4m FOV at 50m range)
That means:
If an object lies within 50 meters distance and is 1.7m to the left or right of the radar’s forward axis, it should be detected. I am okay with some compromise in range if needed, in order to increase the FOV.
What modifications or tuning can I make in the MRR application to increase the azimuth FOV for ?
Can you suggest alternate profiles or example applications using AWR1843AOPEVM that offer wider FOV?
Thanks
Mitesh Singh