Tool/software:
Dear experts,
I am a student conducting experiments to detect human breathing rates at short range (15–20 cm) using a mmWave radar. However, the default vital_signs_AOP_2m.cfg
does not meet my testing requirements — the detected breathing rate is inaccurate or the detection stops altogether.
After completing the Radar Academy training, I used the mmWave Sensing Estimator to modify the chirp configuration. However, when I applied the modified chirp configuration in Industrial Visualizer, the system failed to run and showed the following error:
My questions are as follows:
-
Is this error caused by my modified chirp configuration being incompatible with the "Vital Signs with People Tracking" mode in Industrial Visualizer?
-
For short-range (15–20 cm) breathing detection, are there any other parameters or areas that should be modified to improve detection?
-
Would it be possible to obtain the source code of Industrial Visualizer for further customization?
Best regards,
Tim