This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: Suitable demo for my needs

Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: AWR1843AOP, AWRL1432

Tool/software:

Hello,

I want to monitor traffic and blind spots for motorcycles with a mmwave radar placed at the rear of the motorcycle.

I chose AWR1843AOP for its compact design and I have a AWR1843AOPEVM right now. I have tested demos to got familier with the sdk and radar. 

I want to able to detect motorcycles at 50m range for my system.

Is MRR demo best solution for me or the other demos ? 

I need tracked vehicles x,y,z locations and their speed so I can transmit them via uart and proccess the data. Do I need custom modification on the demo ? 

Do you recommend other radar or AWR1843AOP is still the best for this type of system ? 

Thanks in advance

  • Hello Eren,

    For BSD application specifically, you can check the AWRL1432 which is a better fit and it also comes with a BSD specific EVM and demo as well.
    AWR1843AOP can also be used if its meeting your requirement. With the MRR demo are you able to achieve your use case currently?

    Regards,
    Saswat Kumar