Tool/software:
Hi,
We are trying to understand what is the maximum data recording rate with legacy LVDS mode (Not Aurora).
The data sheet as shown below mentions max speed of 900Mbps per lane (DDR speed of 450Mhz).
There for legacy with two data lanes max total rate for 2 data lanes is 1800Mbps. Is this correct?

However in the DCA1000 user manual states that max rate is 600Mbps for Legacy mode.
Is the limitation of 600Mbps due to the HW on DCA1000 or the AWR2e44p?
How do we configure the LVDS/ DDR clock to 450Mhz so we can get max rate of 900Mbps?
Thanks
Joseph